text.skipToContent text.skipToNavigation

Legrand Offers Custom Installers Complete Solutions with New Brands and Expanded Lines at CEDIA 2016

Features Wide Breadth of Residential CI Products ‘Designed to Be Better’ from Luxul, Middle Atlantic, Nuvo, On-Q, QMotion and Vantage; $10,000 in Product Giveaways


DALLAS, September 14, 2016 – Legrand, the global specialist in electrical and digital building infrastructures, announced a wide array of new products for the residential custom install market from several of its key brands that will be showcased across three booths at CEDIA 2016. Strongly aligned with the company’s corporate focus, “Designed to be Better™,” the combined breadth of these brands provides the dealer with unmatched options and solutions for complete entertainment, comfort and security solutions for the home.

Middle Atlantic (racks, equipment mounting and power solutions), Nuvo (whole home audio systems), On-Q (smart home solutions, infrastructure & AV connectivity), and Vantage (lighting and climate control) will all be featured at booth 5132. Luxul (residential IP networking solutions) will exhibit at booth 4728 and QMotion (advanced shading solutions) at booth 5154.

“Over the last year, Legrand has continued to evolve as an industry leader in power, light, data and digital building infrastructures through a series of acquisitions and expansion of key product lines in the residential custom install space,” said Brian DiBella, president, Electrical Wiring Systems at Legrand North America. “At CEDIA, we will show how we are even better positioned to offer dealers, integrators and home builders the full breadth of products and complete solutions they need to get any residential or light commercial job done.”

Two $5,000 Giveaways Encourage Attendees to Explore Legrand Offerings

Show attendees can become acquainted with each of the company’s residential CI products and breadth of solutions by visiting all three Legrand booths where they can enter to win one of two $5,000 product giveaways. To enter, attendees should stop by any Legrand booth (5132, 5134 and 4728), pick up a passport and visit all three booths to have their passport stamped by Legrand team members.

Those with completed passports, including stamps from Luxul, Middle Atlantic, Nuvo, On-Q, QMotion and Vantage, can hand them in to enter the giveaway. Two winners will be selected over the course of the show. Winners will be announced on all Legrand Twitter accounts on the last day of the show.

Summary of Products Legrand is Exhibiting at its Booths

Luxul (Booth 4728)
Luxul is exhibiting a new series of scalable routers that enable integrators to lay a great foundation for virtually any size network. The company is also showing powerful and easy-to-install switches, which are available with a range of features and form factors—including the elegant AV Series for clean integration with AV rack systems. The Luxul Wireless Controller and Access Points offer seamless roaming, excellent coverage and stellar performance for an outstanding Wi-Fi experience.

Middle Atlantic (Booth 5132):
Middle Atlantic’s new Proximity in-wall box gives installers maximum mounting capacity behind displays with patented Lever Lock™  inside. New Vision Display Mounts provide safe, reliable display mounting with professional features for efficient installation and storage of technology behind the display. RSH Custom Rackshelves are now available in a 1RU design—with patented UMS designs—for small device mounting and an easy, face-after design. Power Distribution with RackLink™, now available in new budget-friendly form factors, lets installers remotely manage projects to save time while adding service value for the customer.

Nuvo (Booth 5132):
The Nuvo Player Portfolio is a whole home audio system designed for the professional market and offers high fidelity sound, no-hassle third-party integration, extensive source variety and complete control with in-wall keypads and iOS and Android devices for maximized listening experiences. The system’s offerings continue to be enhanced with the recently introduced driver for Universal Remote Control (URC) systems, as well as the soon to be introduced P4300 Professional Series Player, soundbar, subwoofer and keypad controller models. Nuvo Series Two, Four and Six speakers are made for professionals and offer models for every space, project and price point.

On-Q (Booth 5132):
The Intuity Home Automation System gives production homebuilders and installers serving the mainstream housing market a cost-effective, modular, repeatable, and affordable solution for controlling entertainment, security, and comfort within a home. It can be operated intuitively and seamlessly via mobile devices, in-wall Command Centers and PCs, and offers easy integration with Legrand’s wide range of high-performing subsystems, as well as those of leading third party manufacturers. On-Q radiant® RF Lighting Control delivers convenient operation with a variety of options, easy installation and simple scene setup from Legrand iOS and Android apps. On-Q Premium High Speed Cables with Ethernet are tested and verified by the Premium HDMI Certification Program and are ensured to deliver the full 18Gbps bandwidth necessary to support 4K UltraHD devices.

QMotion (Booth 5154):
Qadvanced shades with ZigBee Home Automation V1.2 are the only shades with native ZigBee communication capabilities built into the motor, providing robust two-way communication, long battery life and an exclusive manual override feature. Qadvanced Intelligent System Hardwired Shades use CAT-5e or CAT-6 cables for both power and communication, offering industry leading power savings with optional adapters for most pre-wired systems and support of up to 200 devices. Qadvanced Shading Systems are the industry’s narrowest (15 1/2”) and largest (144” x 144” or more with a Qlink system) battery-operated shades, and are designed for a customized experience.

Vantage (Booth 5132):
Vantage’s new Universal Dimming Station and Module provide effective and seamless dimming control of multiple lighting sources in wired or wireless applications. They are load agnostic and offer auto-switching between forward and reverse phase loads. Equinox Touchscreens and Mobile Apps offer consistent user interfaces across all platforms for enhanced interactivity and intuitive lighting, climate, and shade control.

For more information on Legrand and its residential CI products, please click here.


About Legrand

Legrand is the global specialist in electrical and digital building infrastructures.  Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide.  Innovation for a steady flow of new products with high added value is a prime vector for growth, including in particular connectable products enhancing value in use. Legrand reported sales of $5.3 billion in 2015.  Legrand has a strong presence in North America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, QMotion, Quiktron, Raritan, Vantage, Watt Stopper, and Wiremold.  Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). www.legrand.com

#  #  #

 

Media Contacts:

Feintuch Communications
Doug Wright / Richard Roher                                                 
212-808-4903 / 212-808-4902
legrand@feintuchpr.com