What is Indigo-Clean?
LED lighting technology that cleans and disinfects any room by killing a wide variety of pathogens including SARS-CoV-2 and Influenza A while at the same time providing safe illumination for the occupants in the room. It’s as easy as turning on the lights.
How does it work?
Indigo-Clean harnesses the disinfecting property of visible light, specifically 405nm light. Indigo-Clean utilizes a blend of white and 405nm LEDs to illuminate and disinfect a room. This patented blend kills pathogens by oxidizing them from within no matter where they exist – in the air and on surfaces. This blend of LEDs from the visible light spectrum disinfects while occupants are in the room at all times.
What are the benefits?
Since Indigo Clean uses a portion of the visible light spectrum occupants are free to be under these lights all the time. This means that the room is being cleaned and disinfected while the normal day to day activities in any type of room be it a classroom, lobby, office, or conference room are taking place.Supported by third-party research Indigo-Clean is proven to kill a variety of viruses and harmful bacteria. Research performed in partnership with the Icahn School of Medicine at Mount Sinai confirmed Indigo-Clean is effective at killing SARS-CoV-2 and Influenza A. Studies at Maury Regional Medical Center confirmed Indigo-Clean kills harmful bacteria including MRSA and C. diff.
Indigo-Clean technology is incorporated into standard light fixtures making installation and implementation straightforward. Simply look for the Indigo-Clean logo. The light fixtures utilize a blend of white LEDs plus 405nm LEDs providing both ambient light plus disinfecting light from the same fixture.
Where to Use Indigo-Clean
Indigo-Clean can be used in any room at any time. Common applications include bathrooms, lobbies, conference rooms, offices, classrooms and breakrooms. Any time the lights are turned on in these rooms, the disinfecting property of Indigo-Clean is in action.
Indigo-Clean Modes
Luminaires equipped with Indigo Clean technology are available in two different operating modes:
Blended White: white and 405nm LEDs are on at the same time when the room is occupied
Indigo Only: 405nm LEDs are on offering a higher level of disinfection when the room is unoccupied