text.skipToContent text.skipToNavigation

Legrand Expands Furniture Power Offerings Enabling Properties To Deliver Power Wherever Occupant Demand Requires


WEST HARTFORD, CT – January 5, 2018 – Legrand, a global specialist in electrical and network infrastucture solutions, announces an expanded suite of stylish, functional Furniture Power products. This expansion addresses the growing demand for convenient access to power and charging that enables occupants to work, learn and engage seamlessly throughout a property.

“In this constantly connected age, there simply aren’t enough places to stay charged, and searching for power access is a common user frustration,” said Sabrina Snyder, Product Marketing Manager, Wiremold. “By expanding the range of Legrand’s Furniture Power & Charging products, designers and property managers are now able to seamlessly incorporate power into furniture across any spectrum of spaces, whether open floorplan workspaces, classrooms, meeting spaces, lobbies or retail locations.”

Integrated power solutions from Legrand’s designer collections blend power access and optional lighting controls seamlessly in furniture and overall designs. The stylish, diverse options feature quick and easy installation – requiring no drilling – meaning that nearly any piece of furniture can be transformed into a power center that provides immediate mobile device charging for guests.

For properties where more traditional design is required, the newly introduced radiant® Furniture Power Centers ­­bring together refined style and modern convenience. Offering both USB and traditional power capabilities, radiant Power Units are available in two configurations. The Basic Power Units offer charging via tamper-resistant outlets and USB ports, while Switching Power Units integrate outlets and USB port charging alongside a light switch for on/off control of a connected light fixture.

Featuring the astounding array of finishes and intuitive user experiences offered by the adorne® Collection, the newly updated adorne Furniture Power Center now allows for integrated switching and dimming capabilities to deliver added convenience.

The new Desktop Power Center Slim product offers standard power outlets as well as USB ports for charging phones, tablets, and laptops. Available in white/gray as well as black finishes, the Slim product is cord-ended and is an easy retrofit solution to add power to a workstation. Additionally, Legrand deQuorumTM Flip-Up Table Boxes provide flexibility in delivering power and communication connections to work surfaces with sleek, low-profile designs and easy-to-install configurations.

For more information on Legrand Furniture Power solutions, visit https://www.legrand.us/solutions/furniture-power.

 

About Legrand and Legrand, North and Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that includes C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Sanus, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.

 

###

Media Contact:

Kate Henderson
Sharp Communications, Inc.
(212) 829-0002, x105
kh@sharpthink.com