text.skipToContent text.skipToNavigation

Legrand honored by 2019 Cabling Installation & Maintenance Innovators Awards

Five Data Infrastructure Solutions Recognized with Innovators Awards at BICSI Fall 2019

 

West Hartford, Connecticut
October 16th, 2019 

​​​​​​​
Legrand North and Central America, a global innovation leader in power, light, and data technologies for homes, workplaces, and data centers, announced today that its data infrastructure solutions were recognized among the best in the industry by the 2019 Cabling Installation & Maintenance Innovators Awards. The stellar third-party judging panel included cabling and communications system specifiers, designers, integrators and managers with vast professional experience.

Legrand was recognized as a Gold and Silver honoree spanning five separate solutions.

“On behalf of the Cabling Installation & Maintenance Innovators Awards, I would like to congratulate Legrand on their Gold and Silver–level honoree status,” said Cabling Installation & Maintenance’s Chief Editor Patrick McLaughlin. “This competitive, unbiased program celebrates the most original and innovative products in the Industry.”

Intellicore™ – Softawre-Defined Connectivity - Gold

Intellicore utilizes software defined networking (SDN) to offer you an alternative topology in your data center that gives you full software control and software cross connection capability for each fiber “lane” in your fiber network. Intellicore merges SDN with Legrand’s fiber connectivity and physical infrastructure solutions to enable complete software integrated physical networking capability.

LP-Series Power Distribution Units – Gold

Legrand’s new line of LP-Series Power Distribution products offers customers a blended solution of functionality and cost savings. The single-phase line of PDUs comprises of models that can be mounted vertically or horizontally, fitting into most applications found in commercial LAN environments or smaller data centers. Legrand implemented several features into this new line of basic, network-metered or network-switched PDUs that are designed to improve the installation experience and management of a rack’s power distribution.

Clarity® Shielded High Density Jack – Silver

The Clarity Shielded High Density Jack (HDJS) utilizes Legrand’s innovative rear-loading HDJ footprint, allowing for compatible installation into existing HDJ mounting solutions and new shielded modular patch panels. In addition, due to the shared HDJ footprint, fiber and A/V modules can be installed alongside copper modules in any HDJ mounting solution, allowing for mixed media within the same rack unit or device-end mounting solution.

Infinium™ Fiber Splice Cassette – Silver

Legrand’s Splice Cassettes enable fast field termination and provides cable management within the housing. They are designed for use with either Single-Mode (OS2) or Multimode (OM3/OM4) fiber, features 12 or 24 fibers in LC Duplex, LC Quad, or SC Duplex connector styles. Both the 12 and 24 fiber cassettes support fusion splicing of individual or ribbon fibers. Heat shrinks, pigtail slack and cable slack are all managed within the cassette and eliminates the need for individual splice trays or special housings. Splicing can also be done away from the rack housing if needed.

EZ Patch Flat Pack – Silver

With EZ Patch Flat Pack, all the patch cords are laid out flat in a single plastic bag in quantities of 12 or 24 patch cords. Due to the flat package and arrangement of cords there is no cable memory to deal with when removed from the packaging, and a contractor can quickly populate a patch panel without opening multiple bags or removing tie wraps. The result is less overall waste and reduced installation time, simplifying the experience. EZ Patch Flat Pack also comes in standard and reduced (28 AWG) diameters from CAT 5e to CAT 6A. For more information, visit http://www.legrand.us/ortronics/ezpatch

###

About Cabling Installation & Maintenance

Bringing practical business and technical intelligence to today's structured cabling professionals.

For over 20 years, Cabling Installation & Maintenance has provided useful, practical information to professionals responsible for the specification, design, installation and management of structured cabling systems serving enterprise, data center and other environments. These professionals are challenged to stay informed of constantly evolving standards, system-design and installation approaches, product and system capabilities, technologies, as well as applications that rely on high-performance structured cabling systems. Our editors synthesize these complex issues into multiple information products. This portfolio of information products provides concrete detail that improves the efficiency of day-to-day operations, and equips cabling professionals with the perspective that enables strategic planning for networks’ optimum long-term performance.

About Legrand and Legrand, North and Central America

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Drawing on an approach that involves all teams and stakeholders, Legrand is pursuing its strategy of profitable and sustainable growth driven by acquisitions and innovation, with a steady flow of new offerings—including connected products stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand is one of the most sustainable companies in the world, as ranked by the Corporate Knights, and is committed to achieving carbon, water, and waste reductions in its operations, deepening its community relationships, and continuously improving the environmental profile of its products. Legrand reported sales of around $7.1 billion (USD) in 2018. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, www.legrand.us.

# # #