text.skipToContent text.skipToNavigation

Legrand® Launches Code Compliant Wattstopper® 0-10V Decorative Dimmer


SAN JOSE, Calif., July 23, 2018 – Legrand, North and Central America today launched the Wattstopper® DCLV2 0-10V Decorator Dimmer that controls and smoothly dims low voltage lighting loads, including the latest LED and fluorescent fixtures. The DCLV2 is ideal for LED lighting renovations, retrofits, and new construction projects.

The dimmer combines aesthetics and function and can meet advanced energy code requirements. Manual-On or Partial-On settings are what sets the DCLV2 apart from other dimmers. When paired with a Wattstopper ceiling sensor, such as the CI-Series passive infrared (PIR) sensor or DT-Series dual technology sensor and a Wattstopper BZ-150 power pack, the DCLV2 provides a code compliant solution to IECC and ASHRAE 90.1 standards.

Small and medium spaces are well suited for this device including offices, conference rooms, training centers, and classrooms where load control is required from a single location. Benefits and features include:

  • Smooth dimming and easy control for customizing lighting levels in a space.
  • Controls large loads of up to 100 ballasts wired in parallel for larger application spaces.
  • Sensor input for automatic operation and Manual-On and Partial-On mode for code compliance.
  • Compatible with radiant® screwless or standard wall plates for a stylish finishing touch.


“The new DCLV2 dimmer is a stylish device that provides easy control of LED lighting with the added assurance of helping meet new IECC and ASHRAE 90.1 energy requirements,” said David Kaminski, Product Marketing Manager at Legrand. “These benefits along with the clean style and intuitive interface make this dimmer a new favorite for building owners and occupants.”

Code compliant lighting controls simplify the process of meeting code especially as new standards have recently taken effect or will take effect in several cities and states including Wisconsin (IECC 2015), Nevada (IECC 2018), City of Philadelphia (IECC 2018), and Pennsylvania (IECC 2015). In addition to solutions like the DCLV2 dimmer, Legrand has developed design tools that contractors and electrical distributors can use to quickly choose the right solution for their markets.

For design help and examples of lighting controls compliance, please visit: www.legrand.us/solutions/energy-code.  

###
About Wattstopper

Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable, and flexible energy-efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services has been helping customers save energy, meet green initiatives, and comply with energy codes for more than 30 years. legrand.us/wattstopper

About Legrand and Legrand, North & Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $6.2 billion (USD) in 2017. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Milestone AV, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, Projecta, QMotion, Quiktron, Raritan, Sanus, Server Technology, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819)​​​​​​​ www.legrand.us.

###
Media Contact:
Mary Placido,
Legrand Building Control Systems
(415) 218-3627 mary.placido@legrand.us