text.skipToContent text.skipToNavigation

New Riser Diagrams in Wattstopper® DLM Software Simplifies Project Submittal and Quote Process



San Jose, CA, March 1, 2017   – Legrand, North America announced a new riser diagram feature for the Wattstopper LMCS software for configuring Digital Lighting Management (DLM) systems. The riser diagrams provide a detailed layout of the lighting control system showing DLM networked and non-networked devices and connections floor by floor. This feature makes preparing project submittals and quotes easier for designers and technicians, and makes working with larger systems more effective.

The LMCS software simplifies project design and start-up and provides industry professionals with important commissioning documentation, including LEED projects. As each LMCS file contains information about every DLM device, project designers can now use that information to create a one line diagram that shows every DLM device in every room on every DLM Segment. Segment wire to front end hardware will also be shown. The program can generate a system layout of a specific segment or all segments, which can be exported as a multi-page PDF to add to a project submittal or as a multi-layout DXF diagram that can be brought into AutoCAD.

This is one of many new software capabilities and design tools rolled out to ensure success from product start to finish. Other recently announced LMCS features include:
  • Network View provides a holistic view of all DLM networking components on a project allowing for easier design, specification, and layout. It also provides fields for network addresses and other information for better reporting.
  • Bill of Materials can quickly and easily be exported at the area level through the device context menu.
  • Network Bridge Report creates a consolidated report of all room bridges on a single page document.
  • Improved Firmware solves issues resulting from existing bugs.

With the LMCS software, field technicians can easily configure, manage, and update job information while onsite as well as set up advanced features of DLM devices. DLM is an agnostic, intelligent and distributed control system with plug together devices that automatically maximizes lighting energy efficiency.

###


About Wattstopper
Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable and flexible energy efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services have been helping customers save energy, meet green initiatives and comply with energy codes for more than 30 years. www.legrand.us/wattstopper.

About Legrand, North America
Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.3 billion in 2015. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819).www.legrand.us.

###


Media Contact:

Mary Placido, Legrand Building Control Systems
(415) 218-3627 mary.placido@legrand.us