text.skipToContent text.skipToNavigation

Legrand Introduces First Tabletop Speaker For Nuvo Player Portfolio Whole Home Audio System

High Fidelity 2.1 Stereo Speaker, Featuring Built-in Wi-Fi and Remote Control, Delivers Streaming Audio via Wi-Fi, Ethernet or Line Input


Amsterdam
February 7, 2017 


Legrand, the global specialist in electrical and digital building infrastructures, introduced the Nuvo P400, its first tabletop speaker for the Nuvo Player Portfolio, Legrand’s whole home audio system designed by audiophiles for installation by professionals. The sleek model provides pure, clean sound and instant access to content from networked connected devices and popular online streaming services.

The P400 is a powerful 2.1 system, with a five-and a quarter inch woofer, two midrange drivers and two tweeters, providing full, high-fidelity stereo reproduction from a single compact unit. The wide array of streaming services it supports includes Spotify, Pandora, iHeartRadio, TuneIn, Napster, and Deezer.

The new unit, which includes built-in Wi-Fi, an amplifier and speakers, offers multiple control options, enabling music to be easily accessed via its top-mounted, back-lit LED controls, any of the Nuvo Player in-wall keypads, or the convenient Nuvo Player apps for iOS and Android devices.

“The Nuvo P400 tabletop speaker is a crucial piece of our whole home audio system, enabling our solution to accommodate rooms where in-wall speakers or book shelf speakers are not an option,” said Walt Zerbe, Legrand product manager, audio. “Its sleek, modern design fits any space and the fact that it offers the versatility to be used as a single zone or as an addition to as many as 16 zones within the Player Portfolio system makes it very appealing to installers and end-users alike.”

The P400 can be configured as a wired system via Ethernet or wirelessly (802.11 a,b,g,n, 2.4GHz or 5GHz).  It also offers TOSLINK and analog line inputs for connecting an in-room audio source for playback.

The Nuvo P400 speaker will be available in April for an MSRP of $649.99.

 

About Legrand

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.3 billion in 2015. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us. 

#  #  #
 

Media Contacts:

Feintuch Communications
Doug Wright / Richard Roher                         
212-808-4903 / 212-808-4902
legrand@feintuchpr.com