text.skipToContent text.skipToNavigation

Vantage EasyTouch Glass Keypad Now Shipping

Completely Customizable Keypad Combines a Sleek Design With Programmable Buttons for One-Touch Scenes

CARLSBAD, Calif. — April 20, 2020 Legrand's Building Control Systems (BCS) division today announced that the Vantage EasyTouch Glass modular keypad station is now available. The latest keypad combines powerful functionality with a sleek, contemporary design and color options that can be matched with other Legrand products for a consistent look throughout today’s smart homes. 

EasyTouch Glass offers a highly reflective, mirrored look with a smooth-touch tactile surface for a one-of-a-kind aesthetic. The keypad is available with up to five programmable buttons for different scenes — such as “Welcome,” “Away,” or “Party” — allowing users to set the lighting in a space with one touch. With this release EasyTouch Glass becomes the pre-programmed default keypad station within Vantage’s Design Center software — for standard lighting scenes and pre-configured, human-centric Lighting for Life™ scenes. The keypad’s button matrix is also the same as wired or wireless wallbox dimmers, allowing integrators to select the best technology for their application while maintaining a consistent aesthetic.

The keypad can be completely personalized by homeowners, designers, and integrators by mixing or matching colors for trims, buttons, and faceplates, while an inner-surface ink layering process ensures consistent color definition and reflectivity. Buttons are laser-engraved in a TrueType font — now 15% larger, standard — with the letters illuminated by adjustable RGB backlighting in the user’s color of choice. An ambient light sensor automatically adjusts the backlighting based on the time of day, and users can easily determine which scenes are active based on the button’s color or intensity. 

While other solutions separate load and scene functionality into different devices, EasyTouch Glass combines both into a single station, allowing installers to reduce the number of keypads on the walls for a cleaner look. The keypad is easily designed and programmed through Vantage’s Design Center software. Ideal for use as both a stand-alone keypad and in combination with Vantage’s Equinox touchscreens, as well as with wireless applications, the device is simple to install in 1- to 4-gang electrical boxes. 

“Our EasyTouch Glass provides an elegant design to complement the aesthetics of the modern smart home,” said Mark Moody, product manager, Vantage. “In addition, its available color options are matched with other Legrand products including receptacles and nightlights, providing a consistent look above and below the chair rail. And with its programmable buttons and adjustable backlighting, EasyTouch Glass is a world apart from other keypads on the market when it comes to functionality.”

###

About Legrand and Legrand, North and Central America 
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Drawing on an approach that involves all teams and stakeholders, Legrand is pursuing its strategy of profitable and sustainable growth driven by acquisitions and innovation, with a steady flow of new offerings — including connected products stemming from Legrand's global Eliot (Electricity and IoT) program. Legrand is one of the most sustainable companies in the world, as ranked by the Corporate Knights, and is committed to achieving carbon, water, and waste reductions in its operations, deepening its community relationships, and continuously improving the environmental profile of its products. Legrand reported sales of around $7.1 billion (USD) in 2018. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40. www.legrand.us