text.skipToContent text.skipToNavigation

Now Available: Versatile and Economical Wattstopper® FSP-2x2 Fixture Integrated Outdoor Sensors

San Jose, CA, March 15, 2017 – Legrand, North America today announced the availability of the Wattstopper FSP-202 and FSP-212 sensors, the latest IP66-rated additions to the FSP-200 Series line of occupancy sensors with daylight controls. Designed for LED fixtures, these economical, contractor grade sensors meet all code compliant lighting controls requirements.

“The FSP line continues to be the favorite of fixture manufacturers, specifiers, and contractors,” said Daniel Stankovich, Product Manager for Wattstopper at Legrand, North America. “With the availability of our new FSP-202 and FSP-212 products for cost sensitive applications, it is now easier to integrate controls into lighting projects, meet code, and start achieving an additional 30-40 percent in energy savings.”

The sensors are available in low and line voltage options. The FSP-202 operates on 12-32VDC supplied by a power pack, ballast, or driver, and the FSP-212 operates on 120-277VAC. Perfect for pathways, parking lots, parking structures, and high bay applications, the sensors provide multi-level control based on motion and/or daylight contribution, with an option for dusk to dawn daylighting control. A choice of three lenses ensures complete coverage for mounting heights from 8 to 40 feet making the sensor suitable for almost any application.

Set up and installation are easy. Additional features include a choice of five mode options (four operation settings and one service setting) that simplifies sensor configuration. Time delay and light level settings can be adjusted via trimpots on the sensor. The sensors also feature a novel form factor that allows for quicker snap-in installation with a rectangular punch-out. When fully assembled and installed inside a fixture, the FSP-2x2 is IP66-rated for use in wet and cold locations.

FSP-200 series occupancy sensors are the most versatile in the market--simplifying code compliance and meeting the latest parking garage and outdoor lighting control code requirements including California Title 24 (2016) and ASHRAE 90.1 (2010)/IECC (2012).

###

About Wattstopper
​​​​​​​ Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable and flexible energy efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services have been helping customers save energy, meet green initiatives and comply with energy codes for more than 30 years. www.legrand.us/wattstopper.

About Legrand, North America
Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.3 billion in 2015. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). www.legrand.us.

###

Media Contact:
Mary Placido, Legrand Building Control Systems
(415) 218-3627
​​​​​​​mary.placido@legrand.us