text.skipToContent text.skipToNavigation

What is Flex®?
Connectrac Flex® is a versatile, floor-based power and data distribution system that allows users to quickly add or relocate connectivity with ease. The Flex system includes a low-profile raceway and offers two flexible installation options: under carpet tile or on top of flooring surfaces.


How does Flex differ from Connectrac’s Express Kits?
Connectrac’s Express Kits and Flex Raceway System both offer convenient power and data cable management solutions. Express Kits are a compact, ready-to-install power and data kit with a single circuit, ideal for quick setups. Flex, on the other hand, is a highly customizable 4-circuit system, featuring movable power modules, expandable data capacity, and multiple entrance fitting options.


Can Flex support both power and data?
Yes, the Flex raceway system supports both power and data. It accommodates a 4-circuit power system, and data can be added in any required quantity to meet your needs.


Will the Flex raceway or ramps make my furniture uneven?
Flex raceways are designed with a low profile, and the ramps offer a smooth, gradual transition. Most furniture comes with leveling glides that can easily adjust for height, with a maximum adjustment of about ½” if needed.


Are there color options available for Flex?
All Flex power and data devices, along with accessories, come in Dark Gray. For the Flex under-carpet system, all components are completely hidden. In the Flex on-floor system, the visible raceway on top of the floor is available in a Silver or Dark Gray finish.


How are power and data devices spaced along a Flex raceway?
Power devices can be spaced at any 6” increment beyond 2’ on-center, using various standard Powertrac lengths (2’, 3’, 4’, 5’, 6’) and 6” Powertrac Extenders. *For assistance in designing an ideal layout for your project, please contact your local sales representative.


What is the overall height of the Flex raceway?
The installed height of both the Flex Under-Carpet and On-Floor systems is 0.66″.


Are there any length limitations for the Flex raceway?
Yes, Flex raceways can extend up to 75’ from the Entrance Fitting to the end of the raceway. For lengths beyond 75’, simply start a new Flex system using the same type or a different type of entrance fitting to suit your space requirements. 


Are Connectrac Flex and Express Kits ADA-compliant?
Yes, both the Connectrac Flex Raceway Systems and Express Kits meet ADA Accessibility Guidelines. To ensure compliance, receptacles and data boxes should be strategically placed outside paths of travel to maintain accessibility and avoid obstructions.


What is the static load rating of the Flex raceway?
The Flex raceway is designed to handle individual point loads up to 250 lbs. or a 4-point load of 1,000 lbs.


Can Flex be installed in Chicago and New York City?
Yes, as the Connectrac Flex Raceway Systems are UL listed as multioutlet assemblies, they are permitted to be installed in New York City and Chicago. Article 380 of the New York City and Chicago Electrical Codes permits the use of multioutlet assemblies.


Is there a CEU course available for Connectrac Flex?
Yes, we offer AIA and IDCEC-approved CEUs that cover how revolutionary solutions like Flex address power and data needs in agile spaces. To inquire about scheduling a CEU presentation at your location, please email us at info@connectrac.com.


Is Flex UL listed?
Yes, the Connectrac Flex system is cULus listed to UL 111 and CSA C22.2 No. 62 as Multioutlet Assemblies and Fittings.


How many circuits does Flex support?
The Flex system supports a 4-circuit, 7-wire system.


Why does the Flex® Power System have 7 wires instead of 8?
Because Flex was designed with the future in mind.

  • The NEC and UL require only one earth ground per raceway.
  • Following these standards, the ground in the Flex Raceway System is sized for the highest current circuit (20A / 12 AWG).
  • Relevant NEC sections include 215.6, 250.32, 250.121, and 250.122. All Flex electrical components are UL 111-tested to ensure proper ground sizing throughout.

Refer to the Hardwire Device Installation instruction document for more details.


Can Flex wiring be customized?
The Flex raceway uses a prewired, 4-circuit system. While the wiring itself isn’t customizable, the system includes a range of interchangeable power devices that can connect to one or more circuits. These can be hot-swapped as needed, providing virtually unlimited flexibility in configuration.


What gauge wire is used in the Flex 4-circuit power system?
All wired components within the Flex raceway use 12 AWG conductors.


What power device options are available for the Flex system?
Currently, the Flex system offers three power devices:

  • Receptacle Device – a quad outlet with multiple 4-circuit options.
  • Hardwire Device – a 4-circuit unit compatible with most furniture base feeds.
  • Hubcap – provides a walkable surface with easily accessible power for future needs.

How do I switch out Flex power devices?
All Flex power devices are interchangeable and can be hot-swapped using a screwdriver. Simply remove the screws, detach the existing device and snap in the new device of choice.


What types of devices are available?
The standard devices include NEMA 5-20R Receptacle Devices.


Does the Flex system have controlled Receptacle Devices?
Yes, in compliance with California Title 24, ASHRAE 90.1 and other standards, Flex offers split-circuit Receptacle Devices labeled “Controlled” on applicable outlets. Half of these receptacles can be managed by a sensor, timer or other controlling device as required.


Can more than one Hardwire Device be installed in a Flex raceway?
Yes, you can install a Hardwire Device at any Power Hub or Power End Hub location.


What circuit options are available for Flex power devices?
Receptacle Devices come in a variety of single- or split-circuit options, including 1111, 2222, 3333, 4444, 1122, 1144, and 3344 (split-circuit options include controlled receptacles). Additionally, a 4-circuit Hardwire Device is available for use with most furniture-based feeds or similar applications.


Does the Flex system meet scrubwater testing requirements?
Yes, the Connectrac Flex system was evaluated for compliance with the UL 111 Water Exclusion Test.


How many quad devices are allowed per circuit?
There is a maximum of 4 quad devices allowed per circuit.


Can power and data be run together in the Flex raceway?
Yes, the prewired Flex raceway is designed with built-in separation and shielding to safely run power and data cables side-by-side.


What types of data cables are compatible with Flex?
Flex raceways support most standard low-voltage cabling, including Cat 6, Cat 6A, fiber-optic, and others. Cables can be easily added, changed or upgraded by simply lifting off the Top Cover to access the cabling pathway.


How many data cables can fit inside a Flex raceway?
The Flex raceway system has different sizes to support a variety of data needs. Both the under-carpet and on-floor raceways hold up to 4 data cables (e.g., Cat 6), with 2 cables on each side. To expand data capacity, additional Data Channels can be added alongside the main raceway. Each Data Channel can hold up to 10 cables for both under-carpet and on-floor systems, and you can add as many Data Channels as needed to meet your data requirements.


What data device options are available in the Flex system?
The Flex system offers three data devices:

  • Data Device – supports up to 8 low-voltage keystone modules.
  • A/V Device – accommodates any standard double-gang faceplate.
  • Grommet – allows for cable entry and exit within the raceway.


How are data devices attached to the Flex raceway?
All data devices snap securely into either a Powertrac or Data Channel and include screws for additional fastening if needed.


How many cables can terminate in a Data Device?
Each Data Device can hold up to 8 standard RJ45 keystone jacks or other keystone modules. Additionally, Flex offers a Grommet option that allows cables to exit the raceway for easy access to tables, lecterns and other furniture.


Who can install the Flex systems?
A licensed electrical contractor is required to connect the Entrance Fitting’s prewired conduit to the building’s main power supply. All other Flex raceway components can be installed by a facilities team, general contractor, furniture installer, electrical contractor or flooring contractor.


What type of flooring is Flex compatible with?
Flex is available in two installation options—under-carpet and on-floor. The under-carpet system is ideal for carpet tile installations, while the on-floor system works well with hard flooring surfaces.


How is Flex secured to the floor?
Most Flex raceway components are fastened to concrete slabs using concrete screws. For under-carpet installations, MDF Transition Ramps are anchored with pin-anchors, as specified in the installation instructions. Construction adhesive can also be used for initial positioning.


Can Flex raceway components be cut on-site?
While Powertracs and Power Hubs come prewired at specific lengths and cannot be cut, Data Channels, Top Covers and Transition Ramps can be cut to fit as needed.


Can I relocate my Flex system in the future?
Yes, Flex is designed to be easily moved and adapted. Only the wiring connection at the Entrance Fitting requires a licensed electrician. For under-carpet installations, MDF Transition Ramps may need to be replaced, but all other components can simply be unscrewed and relocated.


When in the construction timeline should Flex be installed?
Flex is ideally installed during the electrical rough-in phase, prior to carpet tiling. However, it can be seamlessly integrated at any stage of the construction process, making it suitable for both retrofit and new construction projects.


Can I add additional Flex Powertracs and Power Hubs to an existing raceway?
Yes, the Flex system is designed to be adaptable and expandable. Additional Powertracs and Power Hubs can be easily connected to extend the length of any existing Flex raceway.


How does Flex transition at a Poke-Thru?
The Flex system can be initiated from a 4″ poke-thru that delivers both power and data to the raceway. This specially-designed poke-thru entrance fitting connects to either a power hub or Powertrac corner, allowing the rest of the Flex raceway to be extended from this point.


Can I connect Flex to an existing wall outlet box?
Yes, a 3’ Surface-Mounted Entrance Fitting is available to connect the Flex raceway to an existing wall outlet box.


Have questions or need more information?